ACOUS NAVI monitors the operating status of machine elements by diagnosing the early signs of damage or deterioration. It is available as a PC application and on dedicated hardware.
Our lineup provides condition monitoring and diagnostics for all of NSK's main products–bearings, ball screws, and linear guides.
ACOUS NAVI products utilize NSK-exclusive technologies to analyze vibrations based on the mechanisms behind damage and deterioration based on years of research and development.
NSK’s condition monitoring/diagnostic software ACOUS NAVI is built-in our portable diagnostic devices. ACOUS NAVI will also be available as open platform software.
A compact patrol monitoring device that offers all-in-one high-spec vibration measurements and diagnosis functions.
This is a high-performance wireless device that can measure and diagnose vibrations and the state of rotating machinery on the spot.
Application that offers continuous monitoring when installed on an industrial PC.
A version of the ACOUS NAVI vibration diagnosis application designed for the Internet of Things (IoT) open platform FIELD system developed by FANUC.
“NSK VIRTUAL EXPO” has been finished its session, but due to its popularity you can continue to view it.